FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > A7AY
FAQ
A7AY
1. Can I switch the output to current by using the A7AY while the input is 0 to 10 V?
2. Is the output current for 10 V input the rated current of the inverter?
2. Is the output current for 10 V input the rated current of the inverter?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
1. Yes.
2. The standard set by Pr.56.
2. The standard set by Pr.56.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700