FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Connecting ammeter to output side
FAQ
Connecting ammeter to output side
Can I install an ammeter to the inverter output side?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
Yes.
Use a moving-iron type ammeter.
However, if the carrier frequency exceeds 5 kHz, do not use that meter since an overcurrent losses produced in the internal metal parts of the meter will increase and the meter may burn out.
In this case, use an approximate-effective value type.
You can also connect it between the inverter terminals FM and SD.
Use a moving-iron type ammeter.
However, if the carrier frequency exceeds 5 kHz, do not use that meter since an overcurrent losses produced in the internal metal parts of the meter will increase and the meter may burn out.
In this case, use an approximate-effective value type.
You can also connect it between the inverter terminals FM and SD.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700