FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-Configurator
FAQ
FR-Configurator
When I used the FR Configurator (FR-SW3-SETUP-WJ) setup software to read a stored file, the setting values were already entered.
Is it necessary to perform batch write again to reflect the setting values on the inverter?
Is it necessary to perform batch write again to reflect the setting values on the inverter?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
If the values are already entered in the setting column, performing batch write reflects the setting on the inverter.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700