FAQ


FAQAbout Products
 - FAQ > Drive Products > Inverters-FREQROL > Monitor indicator
 
FAQ
Monitor indicator
      How can I switch the monitor display from the output frequency to output current?  
    
  - Category :
 - 
      
- FAQ > Drive Products > Inverters-FREQROL
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
 - FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
 
 
Answer
    Press the "SET" key once while the output frequency is monitored.
The unit indicator LED changes from "Hz" to "A" and the monitor display changes to the current.
    The unit indicator LED changes from "Hz" to "A" and the monitor display changes to the current.
- Product Name
 - Inverter, magnet motor drive
 
- Product Category
 - Inverter
 
- Series
 - FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700