FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Multi-speed setting and external potentiometer
FAQ
Multi-speed setting and external potentiometer
What are the priorities between multi-speed setting and external potentiometer?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
The multi-speed setting is prioritized.
The external potentiometer setting is effective when the multi-speed signal is not input.
The external potentiometer setting is effective when the multi-speed signal is not input.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700