FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Frequency setting
FAQ
Frequency setting
I want to use the setting dial in the PU operation mode to set the frequency to 65 Hz.
However, when I set Pr.161 (Frequency setting/key lock operation selection) to "1" (potentiometer mode), the setting value stops at 60 Hz even though I turn the setting dial. How can I increase the frequency up to 65 Hz?
However, when I set Pr.161 (Frequency setting/key lock operation selection) to "1" (potentiometer mode), the setting value stops at 60 Hz even though I turn the setting dial. How can I increase the frequency up to 65 Hz?
- Category :
-
- FAQ > Drive Products > Inverters-FREQROL
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ
Answer
The frequency can be set to 65 Hz with the initial setting.
Check if Pr.1 (Maximum frequency) is set to 60 Hz.
Check if Pr.1 (Maximum frequency) is set to 60 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700