FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Unable to communicate via USB connection
FAQ
Unable to communicate via USB connection
A QCPU module and GX Developer or GX Works2 are connected with a USB cable, but they cannot communicate with each other. Are there any remedies?
- Category :
Answer
Check the following points.
(1) Transfer Setup is properly configured.
(2) The USB driver is properly recognized.
(1) Transfer Setup is properly configured.
(2) The USB driver is properly recognized.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)
May I have your opinion?
Related FAQ
- Difference between R and ZR
- How to check scan time
- Updating to the 64-bit Windows 7 version of GX Works2
- Number of modules that can be synchronized using the MELSEC iQ-R series inter-module synchronization function
- Combination of the MELSEC iQ-R series inter-module synchronization function and the fixed scan communication of the multiple CPU system function