Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22550
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/20 15:48
  • Print

Network No., Group No., and Station No. in Network Parameter

In the parameter setting of Ethernet interface module (QJ71E71-100/B2/B5), what do Network No., Group No., and Station No.,
which are in Ethernet/CC IE/MELSECNET cards of Network Parameter, mean?
Category : 

Answer

- Network No. is a number assigned to identify each network when multiple networks are configured. 
  Each network No. must be unique.

- Group No. is a number assigned to group stations in a network.
  Transient transmission allows data to be transmitted to multiple stations in the same group.

- Station No. is a number assigned to identify each network module connected to a network.
  The station No. of each network module must be unique in a network.
Product Name
MELSEC-Q Series
Series
Ethernet Interface Module

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries