Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22557
  • Release Date : 2018/09/03 17:29
  • Update : 2018/09/20 15:53
  • Print

Necessities for the execution environment of MX Component

Does only the developed software need to be installed in a personal computer that is the execution environment of MX Component?
Otherwise, do both the developed software and MX Component need to be installed?
Category : 

Answer

Both the developed software and MX Component must be installed.
Product Name
MELSEC-Q Series
Series
Middleware
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?