FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Recommended cables for MODBUS(R) interface module QJ71MB91
FAQ
Recommended cables for MODBUS(R) interface module QJ71MB91
Which types of cables should be used for QJ71MB91?
- Category :
Answer
The RS-232 cable should meet RS-232 standards and not exceed 15 m in length.
The RS-422/485 cable should meet specifications described in the following manual not exceed 1200 m in length.
- "MODBUS (R) Interface Module User's Manual" Section 3.3.2
The RS-422/485 cable should meet specifications described in the following manual not exceed 1200 m in length.
- "MODBUS (R) Interface Module User's Manual" Section 3.3.2
- Product Name
- MELSEC-Q Series
- Series
- MODBUS
May I have your opinion?
Related FAQ
- Latch settings
- How to read device data and file registers in Q series
- Using the automatic communication function and dedicated instructions at the same time in MODBUS (R) interface module (QJ71MB91)
- Corrective action when the program size exceeds the capacity
- Battery replacement for High-Performance model QCPU