Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22635
  • Release Date : 2018/09/03 17:29
  • Print

Operation error at the execution of a BIN instruction

Are there any methods of preventing an operation error at the execution of a BIN instruction?
Category : 

Answer

Keep SM722 ON or correct the program so that any one of the ten numbers 0 to 9 is stored in each digit of the source data.
An operation error occurs when data other than numbers is stored in each digit of the source data of a BIN instruction.
Product Name
MELSEC-Q Series
Series
CPU
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?