FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > QCPU built-in Ethernet port setting when using the simple PLC communication function
FAQ
QCPU built-in Ethernet port setting when using the simple PLC communication function
What settings are necessary for the built-in Ethernet port QCPU on the external device side when using the simple PLC communication function?
- Category :
Answer
The following settings are required for the "Open Setting" for the number of connected external devices.
- Protocol: "UDP"
- Open System: "MELSOFT connection"
- Protocol: "UDP"
- Open System: "MELSOFT connection"
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)