FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Help window not displayed
FAQ
Help window not displayed
In Windows7, the "Windows Help Support" window is displayed instead of the Help window. Why does this occur?
- Category :
Answer
This occurs because software required to display the Help window is not installed as standard in Windows7. Download the Windows Help program (WinHlp32.exe) for Windows 7 from the Microsoft Support website and install it.
For more details, refer to the technical bulletin FA-A-0091.
For more details, refer to the technical bulletin FA-A-0091.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)
May I have your opinion?
Related FAQ
- How to copy a sheet used by MX Sheet
- Use of an A-compatible 1E frame for the built-in Ethernet port of the built-in Ethernet port QCPU
- Communication between Ethernet and FL-net
- Numbers of devices the automatic communication parameter of the MODBUS(R) interface module accept for writing and reading
- GX Developer's compatibility with 32-bit Windows 7