Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22868
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/22 14:40
  • Print

Program by program difference in comments on display

There are multiple programs and comment files and different comments are displayed from program to program.
Why does this occur?
Category : 

Answer

There are two types of device comments: "global device comment" and "local device comment".

Device comments can be displayed in the ladder editor and Zoom editor windows.
Select [View] -> [Comment] from the menu to display the comments.
When setting both global device comments and local device comments,
select [Tool] -> [Options] -> [Program Editor] -> [Ladder/SFC] -> [Comment] from the menu to set
[Reference/Reflection Target for Device Comment].
Product Name
Engineering Software
Series
Software Package (GPP function)

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries