FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Can I open a program created with GX Works2 in GX Developer?
FAQ
Can I open a program created with GX Works2 in GX Developer?
Can I open an FX program created with GX Works2 in GX Developer?
- Category :
Answer
You cannot open a program in the file format for GX Works2. When saving a project with GX Works2, save it in the format for GX Developer.
(This is possible only when the project type is the simple project and a project is created without labels.)
(This is possible only when the project type is the simple project and a project is created without labels.)
- Product Name
- Engineering Software
- Series
- GX Works2