FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > PLC parameter setting for QJ61BT11N
FAQ
PLC parameter setting for QJ61BT11N
What do I set for "Select" for QJ61BT11N in the I/O assignment setting of the PLC parameter of GX Developer?
- Category :
Answer
If the Network Parameter is used, CC-Link communication does not need the Select setting in the I/O assignment setting of the PLC parameter.
If the parameter is set using a dedicated instruction, the switch setting is required.
If the parameter is set using a dedicated instruction, the switch setting is required.
- Product Name
- Network Related Products
- Series
- CC-Link
May I have your opinion?
Related FAQ
- Detecting the number of disconnections when using QJ71E71-100
- What makes the ERR LED flash in a CC-Link network
- How to set CC-Link reserved stations
- Connecting terminating resistors to the sending end and the receiving end in communication of QJ71C24N
- Executing the QJ71C24N's pre-defined protocol support function