FAQ


FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC iQ-R Series > Motion Controllers > RnMTCPU > Rapid stop signal
FAQ
Rapid stop signal
How long is the deceleration time when "Rapid stop signal" is turned ON?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC iQ-R Series > Motion Controllers > RnMTCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nHCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nCPUN
Answer
The rapid stop deceleration time of parameter block is applied.
However, when the rapid stop deceleration time is set in the servo program, the value is enabled instead of the one in the parameter block.
However, when the rapid stop deceleration time is set in the servo program, the value is enabled instead of the one in the parameter block.
- Product Name
- Motion controller
- Series
- MELSEC iQ-R
MELSEC-Q