Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23560
  • Release Date : 2018/09/14 15:09
  • Print

Minor error 197AH

What is minor error 197AH?
What should I do when it occurs?
Category : 

Answer

Minor error 197AH (Home position return zero not passed) occurs in the following case:
"[St.1066] zero pass" is OFF when the re-movement to the home position is performed by proximity dog, count, and limit switch combined methods, or when the home position return by data set method is started.
Turn the servo motor at least one revolution to pass the zero point.
Execute the home position return with "[St.1066] Zero pass" ON.
Product Name
Motion controller
Series
MELSEC iQ-R
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?