- No : 23601
- Release Date : 2018/09/14 15:09
- 
          
              Print
          
        
 
Degree axis
    
      When the control unit is set to "degree", is it possible to designate the positioning direction other than "shortcut"?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    Yes.
(1) Absolute system
    (a) When the software stroke limit is invalid
        Positioning is carried out in a designated direction by "[Cd.40] ABS direction in 
        degrees". Set "1" or "2" .(Initial value is "0".)
        • 0: Shortcut (direction setting invalid)
        • 1: ABS clockwise
        • 2: ABS counterclockwise
        [Ex.]
         1) Positioning is carried out in a clockwise direction when the current  value  is moved 
            from 315° to 45°.
         2) Positioning is carried out in a counterclockwise direction when the current value is 
            moved from 45° to 315°.
    (b) When the software stroke limit is valid
        The positioning is carried out in a clockwise/counterclockwise direction depending on 
        the software stroke limit range setting method.
(2) Incremental system
    The movement direction is determined by the sign (+, -) of the movement amount.
    (a) For a positive (+) movement direction: Clockwise
    (b) For a negative (-) movement direction: Counterclockwise
  
    
      
        - Product Name
- Simple Motion module/
 Positioning module
        - Series
- MELSEC iQ-R
 MELSEC iQ-F
 MELSEC-Q
 MELSEC-L