- No : 23613
- Release Date : 2018/09/14 15:09
- 
          
              Print
          
        
 
Error 108
    
      What is error 108?
What should I do when it occurs?
    
  
    - Category : 
- 
      
    
 
    Answer
  
    Error 108 (Start not possible) occurs when a start is requested while a stop signal is ON.
Check the "[Md.26] Axis operation status".If  "20: Servo amplifier has not been connected/servo amplifier power OFF" is set, turn ON the control circuit of the servo amplifier.
Be sure not to request a start when the axis operation state is other
than "0: standby", "1: stopped", and "-2: step standby".
  
    
      
        - Product Name
- Simple Motion module/
 Positioning module
        - Series
- MELSEC-Q
 MELSEC-L