FAQ
FAQAbout Products
- FAQ > Drive Products > Geared Motors > Geared Motors Parallel shaft type > About changing the direction of the cable entrance for the terminal box
FAQ
About changing the direction of the cable entrance for the terminal box
Is it possible to change the direction of the cable entrance for the terminal box?
- Category :
-
- FAQ > Drive Products > Geared Motors > Geared Motors Parallel shaft type
- FAQ > Drive Products > Geared Motors > Geared Motors Right angle shaft type
- FAQ > Drive Products > Geared Motors > S-PM Geared Motors Parallel shaft type
- FAQ > Drive Products > Geared Motors > S-PM Geared Motors Right angle shaft type
Answer
Please refer to the section "Terminal box installation location and direction of lead wire outlet" of the general catalogue.
However, GM-J2 series is not supported.
In addition, we can not correspond indoor type (GM-S, GM-SSY, GM-SHY, range from 0.1kW to 0.4kW) using resin terminal box.
However, GM-J2 series is not supported.
In addition, we can not correspond indoor type (GM-S, GM-SSY, GM-SHY, range from 0.1kW to 0.4kW) using resin terminal box.
- Product Name
- Geared Motors
- Series
- Geared Motors Parallel shaft type, Geared Motors Right angle shaft type, S-PM Geared Motors Parallel shaft type, S-PM Geared Motors Right angle shaft type