Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 20779
  • Release Date : 2018/08/21 16:10
  • Print

Regarding service factors

Answer

It is necessary to select the size of the reduction gear section that has mechanical strength equivalent to the output converted to steady load condition taking into consideration various load conditions different depending on the driven machine.

The output converted to steady load condition (kW) = power requirement × service factor
Product Name
Geared Motors
Series
Geared Motors Parallel shaft type, Geared Motors Right angle shaft type, S-PM Geared Motors Parallel shaft type, S-PM Geared Motors Right angle shaft type

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries