FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800/FR-F800
FAQ
FR-A800/FR-F800
The Instruction Manual of the E700 describes that the one rotation of the setting dial is 24 clicks. Is one rotation of the setting dial is also 24 clicks for the 800 series?
- Category :
Answer
It is 30 clicks the FR-A800/FR-F800.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800