FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-A800/FR-F800
FAQ
FR-A800/FR-F800
When the control power supply is continuously energized, will the main circuit undervoltage or instantaneous power failure warning occur when only the main circuit input power supply is cut off with the MC?
- Category :
Answer
When only the main circuit input power supply is cut off with the MC (when the power supply shutoff time is long), the main circuit undervoltage or instantaneous power failure warning does not occur because the power supply shutoff process is performed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800