FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Frequency search
FAQ
Frequency search
When the frequency search is performed by the combination with the general-purpose motor, how many Hz or lower is regarded as 0 Hz?
- Category :
Answer
DC application method (Pr.162 = 0 or 10): 4 Hz or lower is regarded as 0 Hz. AC application method (Pr.162 = 3 or 13): It is not defined since it depends on the electrical characteristic of the motor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800