FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Residual voltage at the output shutoff
FAQ
Residual voltage at the output shutoff
Does the residual voltage at the output shutoff change according to the rotation speed or torque boost?
- Category :
Answer
The rotation speed has almost no effect. The residual voltage increases when the torque boost is increased, but no adjustment is required.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800