FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Error at USB parameter copy
FAQ
Error at USB parameter copy
I copied parameters with a USB memory. When I wrote the copied data to the same model A800, an error of rE5 occurred and the data could not be written. What causes this error?
- Category :
Answer
This error occurs when the parameter file is broken.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800