FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Setting resolution
FAQ
Setting resolution
When Pr.811 is set to "1" or "11", does the setting resolution change according to the control method?
- Category :
Answer
V/F control/Advanced magnetic flux vector control/Sensorless vector control: 0.3 rpm increments, Vector control with encoder: 0.1 rpm increments
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800