FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Parameter copy to the USB memory
FAQ
Parameter copy to the USB memory
Can I write the USB memory parameter copy file (*.cp1) to the inverter when the power supply specification or capacity is different (such as when replacing the FR-A820 with FR-A840)?
- Category :
Answer
Yes. Writing is available when the power supply specification or capacity is different. Note that setting values of the voltage relation is also overwritten according to the voltage difference (200 V/400 V).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800