FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Communication specifications for connection of multiple inverters
FAQ
Communication specifications for connection of multiple inverters
When connecting multiple A series/F series inverters, what terminal should I use for the communication?
- Category :
Answer
Use the RS485 terminal for the multiple communication of the A series/F series inverters.* Communication with the PU connector is only one-to-one connection.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800