FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > FR-A8AP
FAQ
FR-A8AP
When the 24 V complementary type encoder is used, what is the voltage level at ON and OFF of the A8AP?
- Category :
Answer
The ON level is the power supply voltage -3 V or higher and the OFF level is 3 V or lower.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Plug-in option
- Series
- Option