FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Parameter copy to the USB memory
FAQ
Parameter copy to the USB memory
Can I write the USB memory parameter copy file (*.cp1) to the inverter when the model is different (such as when replacing the FR-A800 with FR-F800)?
- Category :
Answer
No. Writing is not available when the model is different. Writing the parameter copy file using a USB memory device is available only for the same models. Otherwise, the error "rE4" is displayed.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800