Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21015
  • Release Date : 2018/08/22 16:25
  • Print

PLC function

What happens with the data when SD1236, 1237, and 1238 overflow?
Category : 

Answer

The maximum values are kept. The values are not cleared to zero.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-A800, FR-F800

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries