FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > Noise filter compliant with the ship classification standards
FAQ
Noise filter compliant with the ship classification standards
Is there any recommended product for the noise filter used with the ship's classification of the FR-A800? Is there a difference in the type of filter depending on the certification authority?
- Category :
Answer
It is recommended to use the noise filter manufactured by Soshin Electric Co., Ltd. There is no difference in the filter type depending on the certification authority. Appropriate noise filter must be selected according to the inverter capacity and rating setting. For details, refer to the sales and service No. 430 in the Mitsubishi Electric FA Global Website, FREQROL NEWS Vol. 48, or Application Catalog for Ships.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800