FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > PLC function
FAQ
PLC function
Pulse train is input from the JOG terminal. What is the count cycle of the sampling pulse number of SD1236?
- Category :
Answer
It is 1 s interval.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800