FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > PLC function
FAQ
PLC function
Can the PLC function be set without FR Configurator2?
- Category :
Answer
No. To set the PLC function, FR Configurator2 is required. (However, the setting cannot be configured with the trial version.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800