FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A800 > PLC function
FAQ
PLC function
Does the PLC function have the performance equivalent to that of typical programmable controllers?
- Category :
Answer
The processing speed, scan time, and others are slower than those of the programmable controllers. There are some restrictions in the number of I/O points, program capacity, number of instructions, and others. For the detail, refer to the Instruction Manual.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A800, FR-F800