FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Electronic bypass function
FAQ
Electronic bypass function
When Pr.138 (Bypass selection at a fault) is set to "1", how can the commercial power supply operation be switched to the inverter-driven operation again?
- Category :
Answer
Turn ON and OFF the RES signal to enable the inverter-driven operation.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700