FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Electronic bypass function
FAQ
Electronic bypass function
Is the electronic bypass sequence function available in the NET operation mode?
- Category :
Answer
No, it is not available. It is only available in the External operation mode or combined operation mode (PU speed command and External operation command (Pr.77 = 3).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A700, FR-F700P, FR-F700