FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > CC-Link communication
FAQ
CC-Link communication
I want to switch the operation mode to NET operation mode to start the inverter and set the frequency in the CC-Link communication, but it does not switch. How should I set the parameters? And I want the operation mode to be fixed to NET operation mode.
- Category :
Answer
After setting Pr.79 (Operation mode selection) to "2" and Pr.340 (Communication startup mode selection) to "10", reset the inverter (or power ON again) to start and fix the mode to NET operation mode.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700