FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Auto tuning
FAQ
Auto tuning
Trips occur due to the electronic thermal O/L relay error.
Does auto tuning help?
Does auto tuning help?
- Category :
Answer
Auto tuning can help to apply appropriate voltage to the load and decrease the current.
Since the electronic thermal O/L relay trips, check that the rated motor current is set correctly in Pr.9 (Electronic thermal O/L relay).
Since the electronic thermal O/L relay trips, check that the rated motor current is set correctly in Pr.9 (Electronic thermal O/L relay).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700