FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Operation panel and FR-PA07
FAQ
Operation panel and FR-PA07
Can I use both the operation panel of E/D700 and FR-PA (PU)07 (PU connector connection)?
- Category :
Answer
Since the operation panel and PU connector cannot be specified for command source at the same time, they cannot be used together.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ