FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Brake resistor
FAQ
Brake resistor
Which terminal should be connected with the brake resistor? Should I remove the jumper of the terminals P and P1?
- Category :
Answer
Connect the brake resistor to the terminal P and terminal PR. (For the FR-A700-7.5K or lower, remove the jumper of the terminals PR and PX.)
Do not remove the jumper of terminals P and P1. (Remove the jumper of the terminals P and P1 when connecting the power factor improving DC reactor.)
Do not remove the jumper of terminals P and P1. (Remove the jumper of the terminals P and P1 when connecting the power factor improving DC reactor.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700