FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Countermeasure against the instantaneous power failure with the inverter
FAQ
Countermeasure against the instantaneous power failure with the inverter
As the countermeasure against the instantaneous power failure with the small type inverter (current model of the FR-A024 and A044), can I supply the power to the control power supply separately?
Even only for the control without operation, is the UPS available?
Even only for the control without operation, is the UPS available?
- Category :
Answer
The power cannot be supplied to the control power supply separately for the FR-A024/A044 and small type FR-E500.
Therefore, the UPS is not available.
Therefore, the UPS is not available.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024, FR-E500