FAQ


FAQAbout Products

- FAQ > Drive Products > Inverters-FREQROL > Range of carrier frequency
FAQ
Range of carrier frequency
How wide is the carrier frequency range?
- Category :
Answer
You can vary the carrier frequency within the range of 0.7 to 14.5 kHz, and it is initially set to 1 kHz that generates low noise and leakage current.
You can change the carrier frequency by Pr.72 (PWM frequency selection).
You can change the carrier frequency by Pr.72 (PWM frequency selection).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A024