FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Start command, speed command
FAQ
Start command, speed command
Can I input the start command via CC-Link and speed command from the terminal 2 of the inverter?
- Category :
Answer
You can do so by setting Pr.339 (Communication speed command source) = 1 (external).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700