FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to changing location of the decimal point and units of the measured value.
FAQ
As to changing location of the decimal point and units of the measured value.
Is it possible to change location of the decimal point or units of the measured value displayed in the Operating mode?
Answer
Since location of the decimal point or units of the measured value displayed is decided by Total load power, it is impossible to change location of the decimal point or units separately. Check [Display of Measured item in the Operation mode] in user's manual detailed edition for the location of the decimal point or units displayed.
The manual is downloaded in this site.
* Total load power is calculated as below:
Total load power(kW) = a x primary voltage(V) x primary current (A) / 1000
(a = Single-phase 2-wire system:1 Single-phase 3-wire system:2 Three-phase 3-wire system:√3 Three-phase 4-wire system:3)
The manual is downloaded in this site.
* Total load power is calculated as below:
Total load power(kW) = a x primary voltage(V) x primary current (A) / 1000
(a = Single-phase 2-wire system:1 Single-phase 3-wire system:2 Three-phase 3-wire system:√3 Three-phase 4-wire system:3)
- Product Name
- Energy Measuring Units
- Series
- EcoMonitorLight
May I have your opinion?
Related FAQ
- As to the current sensor usable for the EcoMonitorPlus (Model: EMU4-BM1-MB, EMU4-HM1-MB, EMU4-A2, EMU4-VA2).
- Extension of current sensor cable (EcoMonitorPlus/Light).
- Recommended replacement cycle for battery (EcoWebServerIII).
- Simultaneous data acquisition of MODBUS RTU communication and Optional Unit.
- As to compensation for power failure (EcoMonitorPlus/Light).