FAQ
FAQAbout Products
FAQ
AX
What is AX (Auxiliary switch)?
Answer
AX (Auxiliary switch) is a switch which electrically displays the ON / OFF state.
The markings are 14/AXa, 12/AXb and 11/AXc.
* If the circuit breaker itself is ON state, 14/AXa and 11/AXc are conductive state.
* If the circuit breaker itself is OFF state or tripping state, 12/AXb and 11/AXc are conductive state.
The markings are 14/AXa, 12/AXb and 11/AXc.
* If the circuit breaker itself is ON state, 14/AXa and 11/AXc are conductive state.
* If the circuit breaker itself is OFF state or tripping state, 12/AXb and 11/AXc are conductive state.
- Product Name
- Internal Accessories
- Series
- WS-V