FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Air Circuit Breakers > ACB test position
FAQ
ACB test position
What does the test position of Drawout type mean?
Answer
The test position is a position where a main circuit is in the "disconnected" state and
only control circuit is in the "connected" state. Control circuit check and ON/OFF operation check can be done without opening/closing a main circuit.
only control circuit is in the "connected" state. Control circuit check and ON/OFF operation check can be done without opening/closing a main circuit.
- Product Name
- Low Voltage Air Circuit Breakers
- Series
- AE-SW