FAQ


FAQAbout Products

- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Air Circuit Breakers > ACB General use Generator protection use
FAQ
ACB General use Generator protection use
What is ACB relay difference between Generator protection(WM) and General protection(WS)?
Answer
General protection relay (WS) of AE-SW type Air Circuit Breaker has tripping characteristic and function for general use. However, we also provide the replay having the special tripping characteristic to protect generator(WM) since ACBs are often used in the generator circuit. WM relay is set at the factory with the specified value in accordance with the rated current and the overload characteristic of the generator, long-time delay current (IL) and the tripping time with 120% of IL is adjustable.
- Product Name
- Low Voltage Air Circuit Breakers
- Series
- AE-SW